13.29.8.2 Effort Level
This setting specifies the duration of the timing-driven phase of optimization during timing-driven Layout. Its value specifies the duration of this phase as a percentage of the default duration. This option is available only when timing constraints have been defined
The default value is 100 and the selectable range is 25 - 500. Reducing the effort level also reduces the run time of timing-driven place-and-route (TDPR). With an effort level of 25, TDPR is almost four times faster. With fewer iterations, however, performance may suffer. Routability may or may not be affected. With an effort level of 200, TDPR is almost two times slower. This variable does not have much effect on timing.