10.2.2.3.2 Input Delays
The delay between the input of the PLL and a given output can be calculated by the following equation. Total Delay = Intrinsic delay +/- feedback delay – mask delay + phase delay + output delay
Intrinsic delay is the total delay of all the muxes and divider elements in the path. This is a fixed value for a given connectivity in a configuration. This delay varies based on the mux selection, frequency values and phase-shifts. Changing the delay element values has no impact on the intrinsic delay.
Feedback delay can be both a positive and a negative delay based on how it is configured.
Mask delay is a fixed system delay to emulate the skew of the CCC, such that the output can be deskewed by selecting this delay.
Output delay is the programmable delay independently selectable for each output.
Phase delay is the shift caused in the output with respect to the input when the VCO output is shifted by one of the 4 possible values of 0, 90, 180 or 270 degrees. This is a function of both input and output frequencies.
The delay calculation is executed using the same values for the software, the Simulation model and Timer such that, for typical, -2 parts under normal operating conditions, these numbers are identical. This enables you to fine-tune your delays by only adjusting the programmable output/feedback delays.