21.14.40.5 Examples
The following example sets all paths between reg1 and reg2 to 3 cycles for setup check. Hold check is measured at the previous edge of the clock at reg2.
set_multicycle_path 3 -from [get_pins {reg1}] –to [get_pins {reg2}]
The following example specifies that four cycles are needed for setup check on all paths starting at the registers in the clock domain ck1. Hold check is further specified with two cycles instead of the three cycles that would have been applied otherwise.
set_multicycle_path 4 -setup -from [get_clocks {ck1}] set_multicycle_path 2 -hold -from [get_clocks {ck1}]