5.30.36.5 Net information report

The section may not appear if there is no net to report. The Net Information Report includes the following sections:

  • List of nets that drive enable flip-flops that have been remapped to a 2-tile implementation
  • List of nets that have been assigned to a chip global resource
  • List of nets that have been assigned to a quadrant global resource
  • List of nets that nets have been assigned to a LocalClock resource using PDC constraints
  • High fanout nets in the post-compile netlist
  • Nets that are candidates for clock assignment and the resulting fanout

If the driver macro of a clock net is fixed in a quadrant clock location then this net will show in the quadrant clock net report.

The number of clock nets (chip+quadrant) can be less than the number reported in the device utilization (such as in the case of PLL using a YB and not the GLB).