21.14.29.3 Description
Removes a multicycle path from the specified clock in the current scenario. If the arguments do not match a multicycle path constraint in the current scenario, or if the specified ID does not refer to a multicycle path constraint, this command fails.
Do not specify both the multicycle path arguments and the constraint ID.