Following a net might take the user to another page or another level in the design. This is
useful when the design spans multiple pages or includes hierarchical logic. To follow a
net, click a net that continues before or after the current page. Nets that continue on
other pages are terminated with a page connector symbol (>).
Note: A net can continue across multiple pages.
Table 16-1. Following Nets
Net
Description
Indicates the net ends on another page
Indicates the net begins on another page
The following figures show two pages including net data_6. On both pages, the net ends with the
page connector symbol (>), indicating the net continues on another page. As stated
earlier, a net can continue across multiple pages.Figure 16-6. Symbol for a Continuing Net 1Figure 16-7. Symbol for a Continuing Net 2