5.4 ECC Fault Injection
To test Fault handling, an EEC error can be generated. Both single and double-bit errors can be generated in both the read and write data paths. Read path Fault injection first reads the Flash data and then modifies them prior to entering the ECC logic. Write path Fault injection modifies the actual data prior to them being written into the target Flash and will cause an EEC error on a subsequent Flash read. The following procedure is used to inject a Fault:
- Load the Flash target address into the ECCADDR register.
- Select 1st Fault bit determined by FLT1PTRx (ECCCONH[7:0]). The target bit is inverted to create the Fault.
- If a double Fault is desired, select the 2nd Fault bit determined by FLT2PTRx
(ECCCONH[15:8]); otherwise, set to all ‘
1’s. - Write 0x55 to NVMKEY.
- Write 0xAA to NVMKEY.
- Set the FLTINJ bit (ECCCONL[0]) in a single operation to enable the ECC Fault injection logic.
- Perform a read or write to the Flash target address.