5.5 Flash OTP by ICSP™ Write Inhibit
ICSP Write Inhibit is an access restriction feature, that when activated, restricts all of Flash memory. Once activated, ICSP Write Inhibit permanently prevents ICSP Flash programming and erase operations, and cannot be deactivated. This feature is intended to prevent alteration of Flash memory contents, with behavior similar to One-Time-Programmable (OTP) devices.
RTSP, including erase and programming operations, is not restricted when ICSP Write Inhibit is activated; however, code to perform these actions must be programmed into the device before ICSP Write Inhibit is activated. This allows for a bootloader-type application to alter Flash contents with ICSP Write Inhibit activated.
Entry into ICSP and Enhanced ICSP modes is not affected by ICSP Write Inhibit. In these
modes, it will continue to be possible to read configuration memory space and any user
memory space regions which are not code-protected. With ICSP writes inhibited, an
attempt to set WR (NVMCON[15]) = 1 will maintain WR =
0, and instead, set WRERR (NVMCON[13]) = 1. All
Enhanced ICSP erase and programming commands will have no effect with self-checked
programming commands returning a FAIL response opcode (PASS if the destination already
exactly matched the requested programming data).
Once ICSP Write Inhibit is activated, it is not possible for a device executing in Debug mode to erase/write Flash, nor can a debug tool switch the device to Production mode. ICSP Write Inhibit should therefore only be activated on devices programmed for production.