30.1 Configuration Bits
In dsPIC33CK512MPT608 family devices, the Configuration Words are implemented as volatile memory. This means that configuration data will get loaded to volatile memory (from the Flash Configuration Words) each time the device is powered up. Configuration data are stored at the end of the on-chip program memory space, known as the Flash Configuration Words. Their specific locations are shown in Table 30-1. The configuration data are automatically loaded from the Flash Configuration Words to the proper Configuration Shadow registers during device Resets.
When creating applications for these devices, users should always specifically allocate the location of the Flash Configuration Words for configuration data in their code for the compiler. This is to make certain that program code is not stored in this address when the code is compiled. Program code executing out of configuration space will cause a device Reset.
| Register Name | Single Partition | Dual Partition, Active | Dual Partition, Inactive | |||
|---|---|---|---|---|---|---|
| 256k Address | 512k Address | 256k Address | 512k Address | 256k Address | 512k Address | |
| FSEC(1) | 0x02BF00 | 0x057F00 | 0x015F00 | 0x02BF00 | 0x415F00 | 0x42BF00 |
| FBSLIM(1) | 0x02BF10 | 0x057F10 | 0x015F10 | 0x02BF10 | 0x415F10 | 0x42BF10 |
| FSIGN(1) | 0x02BF14 | 0x057F14 | 0x015F14 | 0x02BF14 | 0x415F14 | 0x42BF14 |
| FOSCSEL | 0x02BF18 | 0x057F18 | 0x015F18 | 0x02BF18 | 0x415F18 | 0x42BF18 |
| FOSC | 0x02BF1C | 0x057F1C | 0x015F1C | 0x02BF1C | 0x415F1C | 0x42BF1C |
| FWDT | 0x02BF20 | 0x057F20 | 0x015F20 | 0x02BF20 | 0x415F20 | 0x42BF20 |
| FPOR | 0x02BF24 | 0x057F24 | 0x015F24 | 0x02BF24 | 0x415F24 | 0x42BF24 |
| FICD | 0x02BF28 | 0x057F28 | 0x015F28 | 0x02BF28 | 0x415F28 | 0x42BF28 |
| FDMTIVTL | 0x02BF2C | 0x057F2C | 0x015F2C | 0x02BF2C | 0x415F2C | 0x42BF2C |
| FDMTIVTH | 0x02BF30 | 0x057F30 | 0x015F30 | 0x02BF30 | 0x415F30 | 0x42BF30 |
| FDMTCNTL | 0x02BF34 | 0x057F34 | 0x015F34 | 0x02BF34 | 0x415F34 | 0x42BF34 |
| FDMTCNTH | 0x02BF38 | 0x057F38 | 0x015F38 | 0x02BF38 | 0x415F38 | 0x42BF38 |
| FDMT | 0x02BF3C | 0x057F3C | 0x015F3C | 0x02BF3C | 0x415F3C | 0x42BF3C |
| FDEVOPT | 0x02BF40 | 0x057F40 | 0x015F40 | 0x02BF40 | 0x415F40 | 0x42BF40 |
| FALTREG | 0x02BF44 | 0x057F44 | 0x015F44 | 0x02BF44 | 0x415F44 | 0x42BF44 |
| FALTSEQ | 0x02BFFC | 0x057FFC | 0x015FFC | 0x02BFFC | 0x415FFC | 0x42BFFC |
| FBOOT(2) | 0x801800 | |||||
|
Note:
| ||||||