The revision history table describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.
Table 6-1. Revision History| Revision | Date | Description |
|---|
| J | 05/2025 | The following is a summary of the changes made in this revision:- Updated the
document for RT PolarFire® SoC support. The changes are made
throughout the document.
- Updated the descriptions of DELAY_LINE_ DIRECTION and
DELAY_LINE_WIDE ports in Table 4-1.
|
| H | 11/2024 | The following is a summary of the changes made in this revision:- Removed the following sentence from Global Clock Network: The skew is guaranteed to be less than the shortest possible propagation delay.
- Added information about lock signal assertion and de-assertion in the Lock Output section.
- Updated Figure 2-1
and Figure 4-2
by removing the arrow going from the Transceiver block to CCC NE
for indicating that the Transceiver block can drive clock to CCC
SE and not to CCC NE.
- Added a note about the simulation support
limitation in the CCC Simulation Support
section.
|
| G | 05/2024 | The following is a summary of the changes made in this revision:- Added a note about the unused condition of the on-chip oscillators in the On-Chip Oscillators section.
- Added information about the radiation test reports which must be used to decide the CCC PLL usage in RT PolarFire devices. See the Phase-Locked Loops section.
- Added a precautionary note in the Clock Frequency Synthesis section.
|
| F | 11/2023 | Added a note about the usage of 2 MHz RC Oscillator. See On-Chip Oscillators. |
| E | 05/2023 | The following is a summary of the changes made in this revision: |
| D | 12/2022 | The following is a summary of the changes made in this revision: |
| C | 08/2022 | Added information about Resets Outputs On PLL Lock and PLL Lock. See CCC Configuration. |
| B | 04/2022 | The following is a summary of the changes made in this revision: |
| A | 08/2021 | The first publication of the document. This user guide was created by merging the following documents: - UG0684: PolarFire FPGA Clocking Resources User Guide
- UG0913: PolarFire SoC FPGA Clocking Resources User Guide
The revision history tables of both the user guides are retained for the future reference. See Table 2 and Table 3. |
The following revision history table describes the changes that were implemented in the UG0684: PolarFire FPGA Clocking Resources User Guide. The changes are listed by revision.
Note: UG0684: PolarFire FPGA Clocking Resources User Guide is now obsolete and the information in the document has been migrated to PolarFire® FPGA and PolarFire SoC FPGA Clocking Resources User Guide (this document).
Table 6-2. Revision History of UG0684: PolarFire FPGA Clocking Resources User Guide| Revision | Date | Description |
|---|
| Revision 9.0 | 9/20 | The following is a summary of the changes made in this revision:- Information about CCC Configuration was updated.
- Changed PSTRB signal from low to high. See CCC Dynamic Configuration System figure.
- Information about BYPASS_EN_N was removed.
|
| Revision 8.0 | 4/20 | The following is a summary of the changes made in this revision:- Information about External Feedback Mode was updated.
- Information about CCC Configuration was updated.
- Information about Dynamic Phase Shifting was updated.
- Information about Preferred Clock Inputs Connectivity in CCCs was updated.
|
| Revision 7.0 | 8/19 | The following is a summary of the changes made in this revision:- Information about performance of global clock for the transceiver quads was removed and referred to PolarFire FPGA Datasheet.
- Information about Requested Phase field of CCC configurator was added. See CCC Configuration.
- Information about PLL Reference Clock Inputs was updated. See Reference Clock Inputs.
- Information about RC Oscillators Configurator Ports was added.
- Information about Reference Clock Inputs was updated.
- Information related to Libero SoC v12.1 was updated.
|
| Revision 6.0 | 4/19 | Information about minimum input reference frequency for DLL was updated. See DLL Operational Modes. |
| Revision 5.0 | 10/18 | The following is a summary of the changes made in this revision:- Information about PLL reference clock was added. See Reference Clock Inputs.
- Port names were matched according to Libero SoC PolarFire v2.3.
- Information about Internal Post-VCO Feedback Mode, Internal Post-Divider Feedback Mode, and External Feedback Mode was updated.
|
| Revision 4.0 | 5/18 | The following is a summary of the changes made in this revision:- Information about interface clock block was added. See Interface Clock Block.
- Information about global clock networks was updated. See Global Clock Network.
- Information about CCC_SW_CLKIN_W<3:0> was added.
- Information about BIT_SLIP signal was added. See Clock Dividers.
- Information about bandwidth adjustment was updated. See PLL Bandwidth Parameter Settings table.
|
| Revision 3.0 | 12/17 | The following is a summary of the changes made in this revision:- Information about global clock networks was updated.
- The document was updated to include features and enhancements introduced in the Libero SoC PolarFire v2.0 release.
|
| Revision 2.0 | 7/17 | The following is a summary of the changes made in this revision: - Information about PLL/DLL Placement was added. See PLL/DLL Placement.
- Global Clock Network and Clock Sources figure, and System-Level Block Diagram of CCCs figure were updated.
|
| Revision 1.0 | 2/17 | The first publication of UG0684: PolarFire FPGA Clocking Resources User Guide. |
The following revision history table describes the changes that were implemented in the UG0913: PolarFire SoC FPGA Clocking Resources User Guide document. The changes are listed by revision.
Note: UG0913: PolarFire SoC FPGA Clocking Resources User Guide document is now obsolete and the information in the document has been migrated to PolarFire® FPGA and PolarFire SoC FPGA Clocking Resources User Guide.
Table 6-3. Revision History of UG0913: PolarFire SoC FPGA Clocking Resources User Guide| Revision | Date | Description |
|---|
| Revision 3.0 | 7/21 | The following is a summary of the changes made in this revision:- Information about Preferred Clock Inputs Connectivity in CCCs was updated.
- Information about Glitch-Free Clock Switching was updated.
|
| Revision 2.0 | 9/20 | The following is a summary of the changes made in this revision:- Information about CCC Configuration was updated.
- Changed PSTRB signal from low to high. See CCC Dynamic Configuration System figure.
- Information about BYPASS_EN_N was removed.
|
| Revision 1.0 | 4/20 | The first publication of UG0913: PolarFire SoC FPGA Clocking Resources User Guide. |