This bit field defines the pin drive when a fault occurs. The bits have a one-to-one bit
relation to waveform output. If the bit is zero, the pin is tri-states. If the bit is
‘1’, the drive level is according to the setting in the Fault Output
(WEXn.FAULTOUT) registers.
The register cannot be changed if fault protection is enabled (the FDACT bit field in the
FAULTCTRL register is different from NONE).
| Value | Description |
|---|
| 0 |
The pin n (Pxn)
output pad is tri-state |
| 1 |
The pin n (Pxn)
output is overwritten with the value in the FAULTOUT register |