3.4.3.4 Cache Fault Injection
A single-bit error can be injected on any of the data bits of the cache line or the associated
parity bit. The error injection is performed by XORing the data read from the cache line
with a ‘1’. Since the PBU can cache program data from a variety of
address locations depending on the program flow, it is impractical to perform error
injection for a particular program memory fetch address.
The PBU error injection, when enabled with the FLTINJ bit, will cause a one-time error injection the next time the cache memory is accessed by the CPU. The CHESTAT.PAR bit will indicate when the error injection has been performed. At this time, the PBU will also signal that an integrity error has occurred by creating an interrupt event. The user will not be able to determine which line of the cache buffer caused the event and fetch address.
A write to the FLTPTR register while FLTINJ = 1 will have the effect of
re-arming the Fault injection. This will help facilitate a software test routine that
cycles through an error injection on each bit.