22.5.4.3.5 7-Bit Address and Client Read
When a client read is specified by having R/W = 1 in a
7-bit address byte, the process of detecting the device address is similar to that of a
client write, as illustrated in Figure 22-26.
If the addresses match, the following events occur:
- An ACK is generated if the AHEN bit is clear.
- The D/A status bit is cleared, and the R/W status bit is set.
- The module generates the I2CxIF interrupt on the falling edge of the ninth SCLx clock if the CADDRIE (I2CxINTC[10]) bit and CSTIE(I2CxINTC[12]) are enabled.
Because the client is expected to reply with data at this point, it is necessary to suspend the operation of the I2C bus to allow the user software to prepare a response. This is done automatically when the module clears the SCLREL bit. With SCLREL low, the client will pull down the SCLx clock line, causing a Wait on the I2C bus. The SSPND (I2CxSTAT2[31]) bit will be set by the hardware to indicate clock stretching. Packet size (PSZ, I2CxCON2[15:0]) and ND/A needs to be configured and then the user software writes the I2CxTRN register with the response data. SSPND (I2CxSTAT2[31]) bit will be automatically cleared by hardware. If Smart mode (SMEN, I2CxCON2[17]) is disabled, the user must set SCLREL to release the clock or the hardware will automatically set SCLREL to release the clock.
Data setup time (TSU:DAT) can be configured by writing the required setup time to SDASUT(I2CXSDASUT[15:0]) and then enabling SDASUTEN (I2CXSDASUT[31]). In SMART mode (SMEN, I2CxCON2 [17]), hardware will automatically set SCLREL after data setup time.
Once packet size becomes zero, the end of packet (EOP) will be set (I2CxSTAT2[24]).
The SCLREL bit will automatically clear after detecting the client read address, irrespective of the state of the STREN bit.
0)