2.2.4.3 USB_DEVICE_Status Function
C
SYS_STATUS USB_DEVICE_Status(
SYS_MODULE_OBJ object
);
Summary
This function provides the current status of the USB device layer.
Precondition
The USB_DEVICE_Initialize function must have been called before calling this function.
Parameters
| Parameters | Description |
| object | Driver object handle, returned from USB_DEVICE_Initialize |
Returns
SYS_STATUS_READY - Indicates that the device is busy with a previous system level operation and cannot start another.
SYS_STATUS_UNINITIALIZED - Indicates that the device layer is in a deinitialized state.
Example
// This code example shows how the USB_DEVICE_Status function
// can be used to check if the USB Device Layer is ready
// for client operations.
SYS_MODULE_OBJ object; // Returned from DRV_USB_Initialize
SYS_STATUS status;
status = USB_DEVICE_Status(object);
if (SYS_STATUS_READY != status)
{
// Handle error
}
Remarks
None.