2.2.4.35 USB_DEVICE_CONTROL_TRANSFER_RESULT Enumeration
C
typedef enum {
USB_DEVICE_CONTROL_TRANSFER_RESULT_FAILED,
USB_DEVICE_CONTROL_TRANSFER_RESULT_SUCCESS
} USB_DEVICE_CONTROL_TRANSFER_RESULT;
Summary
USB Device Layer Control Transfer Result Enumeration
These enumerated values are the possible return values for control transfer operations. These values are returned by the USB_DEVICE_ControlStatus, USB_DEVICE_ControlSend and the USB_DEVICE_ControlReceive functions.
Members
| Members | Description |
| USB_DEVICE_CONTROL_TRANSFER_RESULT_FAILED | Control transfer failed. This could be because the control transfer handle is no more valid since the control transfer was aborted by host by sending a new setup packet. |
| USB_DEVICE_CONTROL_TRANSFER_RESULT_SUCCESS | Control transfer was successful. |
Remarks
None.