2.2.4.1 USB_DEVICE_Initialize Function
C
SYS_MODULE_OBJ USB_DEVICE_Initialize(
const SYS_MODULE_INDEX instanceIndex,
const SYS_MODULE_INIT * const init
);
Summary
This function initializes an instance of USB device layer, making it ready for clients to open and use it. The number of instances is limited by the value of macro USB_DEVICE_MAX_INSTANCES defined in system_config.h file.
Precondition
None.
Parameters
| Parameters | Description |
| instanceIndex | In case of microcontrollers with multiple USB peripherals, user can create multiple instances of USB device layer. Parameter instanceIndex identifies this instance. |
| init | Pointer to a data structure containing any data necessary to initialize the USB device layer. |
Returns
If successful, returns a valid handle to a device layer object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.
Example
// This code example shows the initialization of the // the USB Device Layer. Note how an endpoint table is // created and assigned. USB_DEVICE_INIT deviceLayerInit; SYS_MODULE_OBJ usbDeviceObj; uint8_t __attribute__((aligned(512))) endpointTable[USB_DEVICE_ENDPOINT_TABLE_SIZE]; // System module initialization deviceLayerInit.moduleInit.value = SYS_MODULE_POWER_RUN_FULL; // Identifies peripheral (PLIB-level) ID deviceLayerInit.usbID = USB_ID_1; // Boolean flag: true -> Stop USB module in Idle Mode deviceLayerInit.stopInIdle = false; // Boolean flag: true -> Suspend USB in Sleep Mode deviceLayerInit.suspendInSleep = false; // Interrupt Source for USB module deviceLayerInit.interruptSource = INT_SOURCE_USB_1; // Number of function drivers registered to this instance of the // USB device layer deviceLayerInit.registeredFuncCount = 1; // Function driver table registered to this instance of the USB device layer deviceLayerInit.registeredFunctions = funcRegistrationTable; // Pointer to USB Descriptor structure deviceLayerInit.usbMasterDescriptor = &usbMasterDescriptor; // Pointer to an endpoint table. deviceLayerInit.endpointTable = endpointTable; // USB device initialization usbDeviceObj = USB_DEVICE_Initialize(USB_DEVICE_INDEX_0, &deviceLayerInit); if (SYS_MODULE_OBJ_INVALID == usbDeviceObj) { // Handle error }
Remarks
This routine must be called before any other USB Device Layer routine is called and after the initialization of USB Device Driver. This routine should only be called once during system initialization.
.