2.2.4.20 USB_DEVICE_EndpointIsStalled Function
C
bool USB_DEVICE_EndpointIsStalled(
USB_DEVICE_HANDLE usbDeviceHandle,
USB_ENDPOINT_ADDRESS endpoint
);
Summary
This function returns the stall status of the specified endpoint and direction.
Precondition
The USB Device should be in a configured state.
Parameters
| Parameters | Description |
| usbDeviceHandle | USB device handle returned by USB_DEVICE_Open |
| endpoint | Specifies the endpoint and direction |
Returns
Returns true if endpoint is stalled, false otherwise.
Example
// This code example shows of how the
// USB_DEVICE_EndpointIsStalled function can be used to obtain the
// stall status of the endpoint 1 and IN direction.
USB_ENDPOINT_ADDRESS ep;
ep = 0x1|USB_EP_DIRECTION_IN;
if(true == USB_DEVICE_EndpointIsStalled (handle, ep))
{
// Endpoint stall is enabled. Clear the stall.
USB_DEVICE_EndpointStallClear(handle, ep);
}
Remarks
None.