2.2.4.16 USB_DEVICE_Attach Function
C
void USB_DEVICE_Attach(
USB_DEVICE_HANDLE usbDeviceHandle
);
Summary
This function will attach the device to the USB. It does this by enabling the pull up resistors on the D+ or D- lines. This function should be called after the USB device layer has generated the USB_DEVICE_EVENT_POWER_DETECTED event.
Precondition
Client handle should be valid. The device layer should have been initialized and an device layer event handler function should have been assigned.
Parameters
| Parameters | Description |
| usbDeviceHandle | Client's USB device layer handle (returned from USB_DEVICE_Open) |
Returns
None.
Example
// This code example shows the set // of steps to follow before attaching the // device on the bus. It is assumed that the // device layer is already initialized. USB_DEVICE_HANDLE usbDeviceHandle; // Get an handle to the USB device layer. usbDeviceHandle = USB_DEVICE_Open( USB_DEVICE_INDEX_0, DRV_IO_INTENT_READWRITE ); if(USB_DEVICE_HANDLE_INVALID == usbDeviceHandle) { // Failed to open handle. // Handle error. } // Register an event handler call back function with device layer // so that we are ready to receive events when the device is // attached to the bus. USB_DEVICE_EventHandlerSet(usbDeviceHandle, APP_USBDeviceEventHandler, NULL); // Now, connect device to USB USB_DEVICE_Attach(usbDeviceHandle);
Remarks
None.