2.2.4.14 USB_DEVICE_RemoteWakeupStop Function
C
void USB_DEVICE_RemoteWakeupStop(
USB_DEVICE_HANDLE usbDeviceHandle
);
Summary
This function will stop the resume signaling. This function should be called after the client has called the USB_DEVICE_RemoteWakeupStart() function.
Precondition
Client handle should be valid. The host should have enabled the Remote Wakeup feature for this device.
Parameters
| Parameters | Description |
| usbDeviceHandle | Client's driver handle (returned from USB_DEVICE_Open) |
Returns
None.
Example
// This code example shows how the device can enable and disable
// Resume signaling on the bus. These function should only be called if the
// device support remote wake-up and the host has enabled this
// feature.
USB_DEVICE_HANDLE usbDeviceHandle;
// Start resume signaling.
USB_DEVICE_RemoteWakeupStart(usbDeviceHandle);
// As per section 7.1.7.7 of the USB specification, device must
// drive resume signaling for at least 1 millisecond but no
// more than 15 milliseconds.
APP_DelayMilliseconds(10);
// Stop resume signaling.
USB_DEVICE_RemoteWakeupStop(usbDeviceHandle);
Remarks
None.