2.2.4.34 USB_DEVICE_CONTROL_STATUS Enumeration
C
typedef enum {
USB_DEVICE_CONTROL_STATUS_OK,
USB_DEVICE_CONTROL_STATUS_ERROR
} USB_DEVICE_CONTROL_STATUS;
Summary
Control Transfer Status Stage Flags
This enumeration defines the flags to be used with the USB_DEVICE_ControlStatus function.
Members
| Members | Description |
| USB_DEVICE_CONTROL_STATUS_OK | Using this flag acknowledges the Control transfer. A Zero Length Packet will be transmitted in the status stage of the control transfer. |
| USB_DEVICE_CONTROL_STATUS_ERROR | Using this flag stalls the control transfer. This flags should be used if the control transfer request needs to be declined. |