23.4 Timing Diagrams
The timing diagrams contained in this section show AHB-Lite non-sequential transfers with 32 bits as the transfer size.
The following diagram shows the AHB-Lite bus signals from fabric interface controller to the fabric slave for a write transaction in bypass mode.
The following diagram shows the AHB-Lite bus signals from the fabric interface controller to the fabric slave for a read transaction in bypass mode.
The following diagram shows the AHB-Lite bus signals from the fabric interface controller to the fabric slave for write transaction in synchronous pipelined mode.
The following diagram shows the AHB-Lite bus signals from the fabric interface controller to the fabric slave for read transaction in synchronous pipelined mode.
The following diagram shows the AHB-Lite bus signals from the fabric master to the fabric interface controller for write transactions in bypass mode. Generation of pipelined requests depends on the efficiency of the master in the fabric to generate it.
The following diagram shows the AHB-Lite bus signals from the fabric master to the fabric interface controller for read transactions in bypass mode. Generation of pipelined requests depends on the efficiency of the master in the fabric to generate it.
The following diagram shows the AHB-Lite bus signals from the fabric master to the fabric interface controller for write transactions in synchronous pipelined mode. Generation of pipelined requests depends on the efficiency of the master in the fabric to generate it.
The following diagram shows the AHB-Lite bus signals from the fabric master to the fabric interface controller for read transactions in synchronous pipelined mode. Generation of pipelined requests depends on the efficiency of the master in the fabric to generate it.