15.3.1 Configuring MSS GPIO Using Libero SoC
This sub-section describes MSS GPIO configuration in Libero SoC and shows different options available for configuring GPIO. MSS GPIO is disabled by default in MSS configurator when the Libero SoC project is created.
Following steps describe how to steps to be used to configure in Libero SoC.
Step 1
Enable MSS GPIO in the Libero SoC project using MSS configurator, as shown in the following figure.
Step 2
Double click GPIO or right click, GPIO and select the configure option to program the GPIOs.