2.52.3 HSMCI_BlockSizeSet Function
C
void HSMCI_BlockSizeSet ( uint16_t blockSize )
Summary
Sets the size of the one data block of transfer
Description
Sets the size of the one data block of transfer.
Precondition
HSMCI_Initialize() must have been called first.
Parameters
Param | Description |
---|---|
blockSize | Size of one block of transfer |
Returns
None.
Example
HSMCI_BlockSizeSet(512);
Remarks
None.