2.52.14 HSMCI_CommandSend Function
C
void HSMCI_CommandSend ( uint8_t opCode, uint32_t argument, uint8_t respType, HSMCI_DataTransferFlags transferFlags )
Summary
This function allows the application to send a SD command on the HSMCI interface
Description
This function is used to send a command on the HSMCI interface and start a transfer.
Precondition
HSMCI_Initialize() must have been called first.
Parameters
Param | Description |
---|---|
opCode | The SD command opcode. |
argument | The argument to the SD command. |
respType | The expected response type for the given SD command. Refer to the HSMCI_CMD_RESP_TYPE enum for the possible values of the response type. |
transferFlags | Transfer flags associated with data transfer Indicates if the transfer contains data stage or not. If the data stage is present, the transferFlags indicate transfer type - single block or multiple block and the transfer direction - read or write |
Returns
None.
Example
HSMCI_DataTransferFlags transferFlags; transferFlags.isDataPresent = false; // Send command 8 with 0x1AAA argument. The expected response is of R7 type. HSMCI_CommandSend(8, 0x1AA, HSMCI_CMD_RESP_R7, transferFlags);
Remarks
The function only supports commonly used SD commands and does not support all the commands specified in the SD protocol.