2.86.2 QMSPIx_ChipSelectSetup Function
C
/* x = QMSPI instance number */
void QMSPIx_ChipSelectSetup(QMSPI_CHIP_SELECT chipSelect)
Summary
Enables the specified hardware chip select
Description
This function allows application to activate the specified chip select. The QMSPI clock phase, clock polarity, baud rate and other settings for the specified hardware chip select become active. This API must be called to switch between multiple hardware chip select lines.
Precondition
The QMSPIx_Initialize() should have been called.
Parameters
chipSelect - One of the hardware chip select from the QMSPI_CHIP_SELECT enum
Returns
None
Example
// Select Chip select 1
QMSPI0_ChipSelectSetup(QMSPI_CHIP_SELECT_1);
Remarks
None.