2.86.4 QMSPIx_TapControlSet Function
C
// x - Instance of the QMSPI peripheral
void QMSPIx_TapControlSet(uint16_t tap_vl, uint32_t tap_ctrl);
Summary
Set control tap adjustment to QMSPI peripheral.
Description
Set control tap adjustment to QMSPI peripheral. This is used to adjust the auto-H/W trim if needed.
Precondition
QMSPI must first be initialized using QMSPIx_Initialize().
Parameters
Param | Description |
---|---|
tap_vl | Tap value to adjust the auto-H/W trim. |
tap_ctrl | Select the tap point for signals, these signals control the interface characteristics |
Returns
None.
Example
QMSPI0_TapControlSet(100, 0);
Remarks
None.