2.102.1 SEFCx_Initialize Function

C

void SEFCx_Initialize( void ) // x - Instance of the SEFC peripheral

Summary

Initializes given instance of the SEFCx peripheral.

Description

This function initializes the given instance of the SEFCx peripheral as configured by the user from within the MCC.

Precondition

None.

Parameters

None.

Returns

None.

Example

SEFC0_Initialize();

Remarks

This function should be called before calling any other SEFCx library function.