2.102.8 SEFCx_RegionLock Function
C
void SEFCx_RegionLock(uint32_t address); // x - Instance of the SEFC peripheral
Summary
Locks a Flash region.
Description
This function is used to lock a certain region of on-chip flash. It takes in address as a parameter and locks the region associated with it.
Precondition
Validate if SEFCx controller is ready to accept new request by calling SEFCx_IsBusy()
Parameters
Param | Description |
---|---|
address | Address of the page to be locked |
Returns
None.
Example
SEFC0_RegionLock(0x00500000);
while(SEFC0_IsBusy());