21.10.3.3 Path Sections
The paths section lists the timing information for different types of paths in the design. This section is reported by default. You can deselect this option in the Timing Report Options dialog box.
By default, the number of paths displayed per set is 5.
You can filter the domains using the Timing Report Options dialog box.
You can also view the stored filter sets in the generated report using the timing report options (see Timing Report Options). The filter sets are listed by name in their appropriate section, and the number of paths reported for the filter set is the same as for the main sets.
By default, the filter sets are not reported.