28.4.6.2.1 Mode 0: PTGITM[1:0] = 0b00
(Continuous Edge Detect with Step Delay at Exit)
In this mode, the selected trigger input is continuously tested starting immediately
after the PTGWHI or PTGWLO command is executed. When
the trigger edge is detected, the command execution completes.
If the step delay counter is enabled, the step delay will be inserted (once) after the valid edge is detected and after the command execution.
If the step delay counter is not enabled, the command will complete after the valid edge is detected and execution of the subsequent command will commence immediately.
PTGWHI or
PTGWLO command execution.Figure 28-3 shows an example timing diagram of Mode 0 operation.