22.5.2.2 Host Transmission
User software should configure data packet size in PSZ (I2CxCON2)
excluding the address byte and PEC, if enabled. The transmission of a data byte, a 7-bit
device address byte or the second byte of a 10-bit address is accomplished by writing
the appropriate value to the I2CxTRN register. Before transmitting,
ND/A (I2CxCON2[18]) has to be cleared/set to an indicated
address/data transmission. Loading the I2CxTRN register will start the following
process:
- The user software loads the I2CxTRN register with the data/address byte to transmit.
- Writing to the I2CxTRN register sets the TBF bit (I2CxSTAT1[0]).
- The data/address byte is shifted out through the SDAx pin until all eight bits are transmitted. Each bit of address or data will be shifted out onto the SDAx pin after the falling edge of SCLx.
- On the ninth SCLx clock, the module shifts in the ACK bit from the client device and writes its value into the ACKSTAT status bit (I2CxSTAT1[15]).
- The module generates the I2CxIF interrupt at the end of the ninth SCLx clock cycle if the HDTXIE (I2CxINTC[1]) bit and HSTIE (I2CxINTC[13]) are enabled.
The module does not generate or validate the data bytes. The contents and usage of the bytes are dependent on the state of the message protocol maintained by the user software.
The sequence of events that occur during the host transmission are provided in Figure 22-8.