11.4.1 I/O Port Control
Before reading and writing any I/O port, the desired pin or pins should be properly configured for the application. Each I/O port has nine registers directly associated with the operation of the port and one control register. Each I/O port pin has a corresponding bit in these registers. Throughout this section, the letter ‘x’ denotes any or all port module instances. For example, TRISx would represent TRISA, TRISB, TRISC and so on. Any bit and its associated data and control registers that are not valid for a particular device will be disabled and will read as zeros.
The TRISx registers configure the data direction flow through port I/O pins. The TRISx register bits determine whether a PORTx I/O pin is an input or an output:
- If a data direction bit is ‘1’, the corresponding I/O port pin is an input.
- If a data direction bit is ‘0’, the corresponding I/O port pin is an output.
A read from a TRISx register reads the last value written to that register. All I/O port pins are defined as inputs after a Power-on Reset (POR).
The PORTx registers allow I/O pins to be accessed; a write to a PORTx register writes to the corresponding LATx register (PORTx data latch). The I/O port pin(s) configured as outputs are updated. A write to a PORTx register is effectively the same as a write to a LATx register. A read from a PORTx register reads the synchronized signal applied to the port I/O pins.
The LATx registers hold data written to port I/O pins; a write to a LATx register latches data to the corresponding port I/O pins. The I/O port pins configured as outputs are updated. A read from a LATx register reads the data held in the PORTx data latch, not from the port I/O pins.