3.3.19.3 mcFlyI_FlyingStart
C
/* Perform flying start */
tmcTypes_StdReturn_e mcFlyI_FlyingStart( tmcFly_Parameters_s * const pParameters,
const float32_t speed, const float32_t commandDirection,
float32_t * const pIdref, float32_t * const pIqref,
bool * const pDutyOverride, int16_t * const pDuty )
Summary
This function performs the Flying Start operation.
Description
This function implements a state machine to manage the flying start process by monitoring rotor speed and applying the appropriate controls to ensure a smooth transition to closed-loop operation. A flying start is used to start a motor that is already spinning, preventing abrupt torque or current spikes.
Precondition
The flying start module must be initialized and enabled.
Parameters
| Param | Description |
|---|---|
| pParameters | A pointer to the flying start module parameter structure. |
| speed | Current speed value. |
| commandDirection | Commanded direction value. |
| pIdref | A pointer to a floating-point variable where the d-axis current reference will be set. |
| pIqref | A pointer to a floating-point variable where the q-axis current reference will be set. |
| pDutyOverride | A pointer to a boolean value indicating whether PWM duty cycle override is active. |
| pDuty | A Pointer to the duty cycle value. |
Returns
Returns status of the flying start process:
- StdReturn_Progress: Operation in progress
- StdReturn_Success: Operation successful
- StdReturn_Fail: Operation failed
- StdReturn_Complete: Operation completed
Example
// Define the flying start module data structure tmcFly_Parameters_s pParameters; float32_t direction = 1.0f; float32_t speed =100.0f; bool pDutyOverride; float32_t iqRef, idRef; int16_t duty[3]; tmcTypes_StdReturn_e status; /** Initialize parameters */ status = mcFlyI_FlyingStart(&pParameters, speed, direction, &idRef, &iqRef, duty); if (status == StdReturn_Complete) { // flying start operation is complete }
Remarks
None.