15.2.2 MSS GPIO Reset Functionality
The MSS GPIO outputs can be reset to a predefined state (logic 1 or logic 0) either by the soft resets coming from the SYSREG block, the Power-on Reset, or the user reset signal (MSS_GPIO_RESET_N) from the FPGA fabric. The selection of the reset can be done through the MSS Configurator in Libero SoC or by writing to reset select registers of the SYSREG block. See Table 15-10 for reset select signals.
Following are the two reset resources of the MSS GPIO block:
- Hard reset:
- The MSS_GPIO_RESET_N is a reset signal generated from the FPGA fabric
- Power-on reset is a device reset signal
- Soft reset from the SYSREG block: There are two soft reset signals generated from the SYSREG block: one for the output registers and another for the input and interrupt registers.
- The MSS_GPIO_SOFTRESET is a soft reset signal from the SYSREG block for the MSS GPIO block input registers (GPIO_IN) and interrupt registers (GPIO_IRQ)
- There are four byte-wise soft reset signals from the SYSREG block to reset all the 32 GPIO output registers. Each soft reset signal resets the GPIO output byte (8-GPIO_OUT registers). Table 15-6 shows the soft reset signals from the SYSREG block
Each GPIO output byte reset is enabled by the control signals from the SYSREG block. The reset enable feature for each GPIO output byte is used to hold the GPIO_OUT register values from not getting affected by the reset source.
The GPIO output byte reset configuration in Libero SoC is explained in the Initializing the MSS GPIO.