2.7.3.4 SysTick Calibration Value Register
The SYST_CALIB register indicates the SysTick calibration properties. See the register summary in Table 2-65 for its attributes. The bit assignments are:
| Bits | Name | Function |
|---|---|---|
| [31] | NOREF | Reads as one. Indicates that no separate reference clock is provided. |
| [30] | SKEW | Reads as one. Calibration value for the 10ms inexact timing is not known because TENMS is not known. This can affect the suitability of SysTick as a software real time clock. |
| [29:24] | Reserved. | |
| [23:0] | TENMS | Reads as zero. Indicates calibration value is not known. |
If calibration information is not known, calculate the calibration value required from the frequency of the processor clock or external clock.