2.7.4 Memory Protection Unit
This section describes the Memory protection unit (MPU).
The MPU divides the memory map into a number of regions, and defines the location, size, access permissions, and memory attributes of each region. It supports:
- independent attribute settings for each region
- overlapping regions
- export of memory attributes to the system.
The memory attributes affect the behavior of memory accesses to the region. The Cortex-M3 processor MPU defines:
- eight separate memory regions, 0-7
- a background region.
When memory regions overlap, a memory access is affected by the attributes of the region with the highest number. For example, the attributes for region 7 take precedence over the attributes of any region that overlaps region 7.
The background region has the same memory access attributes as the default memory map, but is accessible from privileged software only.
The Cortex-M3 processor MPU memory map is unified. This means instruction accesses and data accesses have same region settings.
If a program accesses a memory location that is prohibited by the MPU, the processor generates a MemManage fault. This causes a fault exception, and might cause termination of the process in an OS environment.
In an OS environment, the kernel can update the MPU region setting dynamically based on the process to be executed. Typically, an embedded OS uses the MPU for memory protection.
Configuration of MPU regions is based on memory types, see Memory Regions, Types and Attributes.
The following table shows the possible MPU region attributes. These include shareability and cache behavior attributes that are not relevant to most microcontroller implementations. See MPU Configuration for a Microcontroller for guidelines for programming such an implementation.
| Memory Type | Shareability | Other Attributes | Description |
|---|---|---|---|
| Strongly- ordered | All accesses to Strongly-ordered memory occur in program order. All Strongly-ordered regions are assumed to be shared. | ||
| Device | Shared | Memory-mapped peripherals that several processors share. | |
| Non-shared | Memory-mapped peripherals that only a single processor uses. | ||
| Normal | Shared | Non-cacheable Write-through Cacheable Write-back Cacheable | Normal memory that is shared between several processors. |
| Non-shared | Non-cacheable Write-through Cacheable Write-back Cacheable | Normal memory that only a single processor uses. |
Use the MPU registers to define the MPU regions and their attributes. The MPU registers are:
| Address | Name | Type | Required privilege | Reset value | See |
|---|---|---|---|---|---|
| 0xE000ED90 | MPU_TYPE | RO | Privileged | 0x00000800 | MPU Type Register |
| 0xE000ED94 | MPU_CTRL | RW | Privileged | 0x00000000 | MPU Control Register |
| 0xE000ED98 | MPU_RNR | RW | Privileged | 0x00000000 | MPU Region Number Register |
| 0xE000ED9C | MPU_RBAR | RW | Privileged | 0x00000000 | MPU Region Base Address Register |
| 0xE000EDA0 | MPU_RASR | RW | Privileged | 0x00000000 | MPU Region Attribute and Size Register |
| 0xE000EDA4 | MPU_RBAR_A1 | RW | Privileged | 0x00000000 | Alias of MPU_RBAR, see MPU Region Base Address Register |
| 0xE000EDA8 | MPU_RASR_A1 | RW | Privileged | 0x00000000 | Alias of MPU_RASR, see MPU Region Attribute and Size Register |
| 0xE000EDAC | MPU_RBAR_A2 | RW | Privileged | 0x00000000 | Alias of MPU_RBAR, see MPU Region Base Address Register |
| 0xE000EDB0 | MPU_RASR_A2 | RW | Privileged | 0x00000000 | Alias of MPU_RASR, see MPU Region Attribute and Size Register |
| 0xE000EDB4 | MPU_RBAR_A3 | RW | Privileged | 0x00000000 | Alias of MPU_RBAR, see MPU Region Base Address Register |
| 0xE000EDB8 | MPU_RASR_A3 | RW | Privileged | 0x00000000 | Alias of MPU_RASR, see MPU Region Attribute and Size Register |