2.10.31 CCPx_Compare16bitPeriodValueGet Function

C

/* x = CCP instance number */

uint16_t CCPx_Compare16bitPeriodValueGet( void )

Summary

Reads the period value of given timer.

Description

This function reads the value of period.

Precondition

CCPx_CompareInitialize() function must have been called first.

Parameters

None.

Returns

uint16_t - The timer's period value.

Example

uint16_t period = 0;
CCP1_CompareInitialize();
period = CCP1_Compare16bitPeriodValueGet();

Remarks

The caller must know the number of significant bytes of timer. Period value is right-aligned.