2.10.23 CCPx_Compare32bitPeriodValueGet Function
C
/* x = CCP instance number */
uint32_t CCPx_Compare32bitPeriodValueGet( void )
Summary
Reads the period value of given timer.
Description
This function reads the value of period.
Precondition
CCPx_CompareInitialize() function must have been called first.
Parameters
None.
Returns
uint32_t - The timer's period value.
Example
uint32_t period = 0;
CCP1_CompareInitialize();
period = CCP1_Compare32bitPeriodValueGet();
Remarks
The caller must know the number of significant bytes of timer. Period value is right-aligned.