2.88.12 RAM_ECC_FaultCaptureAddrGet Function

C

uint32_t RAM_ECC_FaultCaptureAddrGet(void)

Summary

Returns the address of the captured ECC fault.

Description

This function returns the address where the last ECC fault was detected in the RAM, as stored in the MCRAMC_ERRCADR register.

Precondition

None

Parameters

None

Returns

returns the fault address

Example

uint32_t faultAddress;

// Get the address of the captured ECC fault
faultAddress = RAM_ECC_FaultCaptureAddrGet();