2.88.11 RAM_ECC_FaultCaptureParityGet Function

C

uint8_t RAM_ECC_FaultCaptureParityGet(void)

Summary

Returns the parity of the captured ECC fault.

Description

This function returns the parity value associated with the most recent ECC fault detected in the RAM.

Precondition

None

Parameters

None

Returns

parity value of ECC fault.

Example

uint8_t faultParity;

// Get the parity value of the captured ECC fault
faultParity = RAM_ECC_FaultCaptureParityGet();