2.51.61 GPIO_POLARITY Enum

C

The GPIO_POLARITY vary based on device family. Refer to the generated header file for the actual values.

Summary

This enum is used to to specify the pin polarity in the GPIO_PinPolarityConfig API

Description

This enum is used to to specify the pin polarity in the GPIO_PinPolarityConfig API

Remarks

None