2.51.24 GPIO_PinGroupOutputEnable Function
C
void GPIO_PinGroupOutputEnable(GPIO_PIN pin)
Summary
Enables the group output of the given GPIO pin
Description
Every GPIO has two mechanisms to set a GPIO data output - either using the grouped GPIO output register or using the single GPIO output data bit located in the Pin Control register. This API enables control of the GPIO pin using the grouped GPIO output register.
Precondition
None.
Parameters
Param | Description |
---|---|
pin | One of the GPIO pins from the enum GPIO_PIN |
Returns
None
Example
GPIO_PinGroupOutputEnable(GPIO_PIN_GPIO012);
Remarks
None