2.51.59 GPIO_FUNCTION Enum

C

The GPIO_FUNCTION vary based on device family. Refer to the generated header file for the actual values.

Summary

This enum is used to to specify the GPIO pin function to configure a pin to using the GPIO_PinMUXConfig API

Description

This enum is used to to specify the GPIO pin function to configure a pin to using the GPIO_PinMUXConfig API

Remarks

None