2.51.57 GPIO_DIR Enum
C
The GPIO_DIR vary based on device family. Refer to the generated header file for the actual values.
Summary
This enum is used to to specify the GPIO pin direction in the GPIO_PinDirConfig API
Description
This enum is used to to specify the GPIO pin direction in the GPIO_PinDirConfig API
Remarks
None