2.51.42 GPIO_GroupRead Function

C

uint32_t GPIO_GroupRead(GPIO_GROUP group, uint32_t mask)

Summary

Returns the value of the given GPIO group.

Description

Returns the state of the pins in the given GPIO group

Precondition

None

Parameters

ParamDescription
groupOne of the pin groups from the enum GPIO_GROUP
maskBit wise OR of pins whose input needs to be returned

Returns

A 32-bit value indicating the status of pins corresponding to the mask value passed to the API

Example

// Read the value of pins GPIO_007, GPIO_034.
uint32_t group_read_val = GPIO_GroupRead(GPIO_GROUP_0, 0x10000010);

Remarks

None