2.51.62 GPIO_PROPERTY Enum
C
The GPIO_PROPERTY vary based on device family. Refer to the generated header file for the actual values.
Summary
This enum is used to to specify the property of the pin to configure in the GPIO_PropertySet API
Description
This enum is used to to specify the property of the pin to configure in the GPIO_PropertySet API
Remarks
None