2.51.10 GPIO_PortOutputEnable Function

C

void GPIO_PortOutputEnable(GPIO_PORT port, uint32_t mask)

Summary

Enables selected IO pins of a port as output(s).

Description

This function enables selected IO pins of the given port as output(s).

Precondition

None.

Parameters

ParamDescription
portOne of the IO ports from the enum GPIO_PORT
maskA 32 bit value in which positions of 0s and 1s decide which IO pins of the selected port will be setup as outputs.
  • 1's Will set corresponding IO pins as output(s).

  • 0's Will cause the direction of the corresponding IO pins to remain unchanged.

Returns

None.

Example

// Make RC5 and RC7 pins as output
GPIO_PortOutputEnable(GPIO_PORT_C, 0x00A0);

Remarks

None.