2.51.58 GPIO_DRV Enum

C

The GPIO_DRV vary based on device family. Refer to the generated header file for the actual values.

Summary

This enum is used to to specify the pin drive strength in the GPIO_DrvStrConfig API

Description

This enum is used to to specify the pin drive strength in the GPIO_DrvStrConfig API

Remarks

None