2.51.64 GPIO_PWRGATE Enum
C
The GPIO_PWRGATE vary based on device family. Refer to the generated header file for the actual values.
Summary
This enum is used to to specify the power well for the pin in the GPIO_PinPwrGateConfig API
Description
This enum is used to to specify the power well for the pin in the GPIO_PinPwrGateConfig API
Remarks
None