2.51.35 GPIO_PinPolarityConfig Function

C

void GPIO_PinPolarityConfig(GPIO_PIN pin, GPIO_POLARITY polarity)

Summary

Configures the polarity of the given GPIO pin

Description

This API lets the application configure the polarity of the given GPIO pin

Precondition

The pin function must be set to other than GPIO

Parameters

ParamDescription
pinOne of the values from the enum GPIO_PIN
polarityOne of the values from the enum GPIO_POLARITY

Returns

None

Example

GPIO_PinPolarityConfig(GPIO_PIN_GPIO012, GPIO_POLARITY_INVERTED);

Remarks

None